FB#.IDENTIFIED

Description

This parameter is set according to FB#.SELECT on drive power up if FB#.SELECT is not –1; otherwise the parameter value is read from the drive memory.

Type

Description

0

No feedback identified
1 No Encoder

10

Incremental Encoder with A/B Quad, marker pulse with Halls

11

Incremental Encoder with A/B Quad, marker pulse without Halls

13 Step/Direction
14 Clockwise/Counter-Clockwise

20

Sine Encoder with marker pulse with Halls

21

Sine Encoder with marker pulse without Halls

30

EnDat Analog with Sine Cosine

31

EnDat Digital

34

BiSSClosed"Bi-directional Serial Synchronous interface" An open-source communication protocol for feedback devices. With BiSS, all of the computation for interpolation in regard to position occurs on the ASIC directly in the encoder-C

40

Resolver

41

SFD (Smart Feedback DeviceClosedA process whereby some proportion of the output signal of a system is passed (fed back) to the input. In automation, a device coupled to each motor to provide indication of the motor's shaft angle, for use in commutating the motor and controlling its speed and position)

45 SFD3 (Smart Feedback Device Gen 3)
46 HIPERFACE DSL
110 SFA - Incremental Encoder with Halls
111 SFA - Incremental Encoder without Halls
120 SFA - Sine Encoder with Halls
121 SFA - Sine Encoder without Halls
130 SFA - EnDat Analog
131 SFA - EnDat Digital
134 SFA - BiSS-C Digital
140 SFA - Resolver
141 SFA - SFD (Smart Feedback Device)

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

N/A

Range

N/A

Default Value

N/A

Data Type

Integer

See Also

FB#.SELECT

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen